Welcome Aboard
https://uop.stage.honeywell.com/en/search

CONVERT WASTE HEAT INTO VALUABLE ENERGY

Patented Qpinch Heat Transformer (QHT) technology upgrades waste heat into industrial heat to provide energy efficiency, OpEx saving and reduce carbon emissions(*).

Connect with an expert

Increase Energy Efficiency Reusing Waste Heat

In collaboration with Honeywell UOP and Qpinch, Qpinch Heat Transformer (QHT) offers an innovative solution which combines efficiency and flexibility. This unique combination allows the technology to be integrated into just about any site.  It transforms waste heat into upgraded valuable  process heat, with very little  electricity consumption, providing the best financials within its technology category.

(*) If the upgraded heat is used to offset heat input derived from the combustion of fossil fuels this can result in a positive impact on one’s CO2 emissions.

Latent heat recovery is advancing industrial energy efficiency by capturing and repurposing heat that would otherwise be lost.

Revolution of Latent Heat Recovery

Latent heat recovery is advancing industrial energy efficiency by capturing and repurposing heat that would otherwise be lost. In many processes, significant energy is wasted through hot exhaust gases or excess steam. By harnessing this latent heat—energy stored during phase changes such as condensation—industries can dramatically reduce energy consumption, operating costs and carbon emissions if the upgraded heat is used to replace the combustion of fossil fuels.

  • Refining
  • Petrochemicals
  • Gas Processing
  • Renewables
  • Carbon Capture
  • Specialty Chemicals

With rising energy prices and increasing pressure to meet sustainability goals, latent heat recovery is becoming a strategic priority aligned with energy efficiency and decarbonization. Companies in energy-intensive sectors are recognizing that improving heat recovery isn’t just about cost savings—it’s also about long-term competitiveness and resilience against energy market volatility.

Integrating latent heat recovery enhances process efficiency and operational stability. By reducing reliance on external energy sources, companies can mitigate supply chain risks and improve energy security.

The QHT Advantage

Minimal Maintenance: A Qpinch Heat Transformer is built with industry-standard components that uses no compressors, making the installation highly efficient and with low-maintenance requirements.

Safety Compliance and Sustainability: The QHT complies with strict industry safety regulations, and is a proven technology backed by 14 years of research and development. The QHT operates without chemical consumption or use of catalysts. As a bonus, the implementation of heat recovery systems may qualify plants for incentives, credits or certificates.

Flexible Technology: The QHT can cope with a wide range of temperature fluctuations, operating from 10% to 100% of design duty, all with limited need for operator intervention. The technology allows for the combination of multiple heat sources and varying output temperature.

Low OpEx - High Yield: The combination of marginal electricity requirements and low-maintenance demands of the QHT, results in the most efficient process steam output for the money invested: a maximum 40kW of electricity per MW steam.

QHT modular construction with cutting-edge technology

Modular construction is transforming the industrial landscape by offering faster, more cost-effective, and scalable solutions. By constructing pre-engineered modules offsite, companies can significantly reduce installation time, minimize disruptions, and ensure higher quality through controlled fabrication. This approach is particularly valuable in energy-intensive industries, where efficiency, reliability, and rapid deployment are critical.

Honeywell UOP's Streamlined Risk-Mitigated Approach Empowered by Qpinch Technology

Honeywell UOP and Qpinch solutions offer enhanced energy efficiency, lower CO2 emissions (when the upgraded heat is utilized to offset fossil fuel combustion elsewhere in the facility), and reduced operating costs.  As industries pursue sustainable and high-performance solutions, Honeywell UOP is enabling  a new benchmark for efficiency and innovation, guiding clients toward a more energy-efficient future.

Ready to Connect?

Get in Touch with our technical experts

Let’s Talk

REQUEST SUPPORT

CONTACT SALES